Systems.xml File Attributes

When you use the Configure Connections tool to configure a client - system connection, the settings you define are saved within the auto-generated Systems.xml file as attributes and values. If you create or edit a Systems.xml file manually, you can include the attributes in your file and also define their values.

Many of the elements in a Systems.xml file have attributes for which you can set values. The attributes correspond to the settings on the Configure Connections tool and the various displays that you can access via the Configure Connections tool, such as the Advanced Settings window.

For each of the elements, you need to define or edit the attributes correctly:

XML is case-sensitive. To be valid in XML files, Boolean 'true' and 'false' values must be fully lower case.

When you use the Configure Connections tool to configure a connection, the resulting Systems.xml file contains auto-generated <opcdaclsid>, <opchdaclsid>, and <opcaeclsid> elements. These elements can allow third-party OPC clients to connect to a system and can only be included as part of a Geo SCADA Expert generated Systems.xml file. You cannot include them in manually edited Systems.xml files - you should use the Configure Connections tool to configure third-party OPC Client connections (see Third-Party OPC Client - System Connections).

Example: Systems.xml file for a ViewX client with Connections to 2 Servers

The following example shows the contents of a valid Systems.xml file for a ViewX client that is connected to a single logical database called "Main". The logical database "MAIN" is implemented on two servers called "TAPC04" and "TAPC06" respectively:

<Systems>

<Default system="MAIN"/>

<System name="MAIN" type="SCX" enabled="true" visibleInViewX="true" clientLicensing="true" synchronizedOnly="false" validateServerCert="true" clientCertMode="2" selectClientCertBySubjectSubString="abc" workstationName="CentralSite Area C PC3" defaultSystemPriority="5">

<Server name="TAPC04" cost="6" port="5481" compress="false" connectTimeout="30000" requestTimeout="120000" disconnectTimeout="30000" pollInterval="10" pollTimeout="15000">

</Server>

<Server name="TAPC06" cost="8" port="5481" compress="false" connectTimeout="30000" requestTimeout="120000" disconnectTimeout="30000" pollInterval="10" pollTimeout="15000">

</Server>

</System>

</Systems>