Configure Modbus Properties

This section only applies if the SCADAPack E outstation is a Modbus Slave. To communicate as a Modbus Slave device, at least one of the SCADAPack E outstation’s ports has to have its Function defined as Modbus Slave (see Configure the Properties of the Individual Ports). If the outstation is not configured as a Modbus Slave, Geo SCADA Expert will ignore the settings in this section of the Form.

Use the fields in the Modbus section of the SCADAPack tab to specify these properties: