Configure the Properties of the Individual Ports

Ensure that you Specify the Outstation Type before configuring the properties on the Ports section of the Outstation Type tab.

Use the fields within the Ports section of the Outstation Type tab to specify the configuration of the serial ports on the SCADAPack E outstation. The number of ports and configuration fields vary, depending on the Outstation Type that is specified at the top of the tab (see Specify the Outstation Type).

This section details the most common SCADAPack E outstation port settings. For a complete description of the available port settings, see the SCADAPack E Configuration Technical User and Reference Manual, and the SCADAPack E Communication Interfaces Technical User and Reference Manual.

Although Geo SCADA Expert is capable of setting the outstation’s port configuration by downloading the outstation’s configuration, Geo SCADA Expert first has to be able to communicate with the outstation. To enable this, use the E Configurator to initially configure one of the outstation’s ports and its DNP3 address, to allow Geo SCADA Expert to communicate with it.