Use a Certificate for an AVEVA Insight Connection Token
Before you connect Geo SCADA Expert to AVEVA Insight (formerly Wonderware Online), you have to enter a connection token in Geo SCADA Expert (see Exporting Historical Data to AVEVA Insight and see Set Token). This enables you to encrypt the communications between the two applications.
You can only use the connection token on the computer that you used to generate it. Therefore, if your Geo SCADA Expert system has a Hot Standby configuration, you also have to use a certificate so that the connection token can be shared by more than one computer. You have to do this on the Hot-Standby servers in your system.
There are two types of certificate that you can use:
- Trusted Authority certificate—You obtain such a certificate from a certificate authority (CA), such as VeriSign, GlobalSign, DigiCert, GoDaddy, and StartCom. We strongly recommend that you use trusted certificates with Geo SCADA Expert.
- Non-trusted self-signed certificate—A non-trusted certificate does not provide authentication. The client cannot tell if the certificate is legitimate.
You can either:
- Obtain a public signed certificate from a zero cost provider.
- Create a self-signed certificate.
For more information, see the Geo SCADA Expert Knowledge Base.
The supported certificate formats are those that are supported by Windows.
SECURITY RISK
Before you can use the certificate, you have to contact AVEVA Insight Support and register the public certificate with them. You then have to install the certificate into the local machine certificate store.
To use a certificate, follow this procedure:
- Open Windows Certificate Manager for the local machine. To do this, enter the text certlm.msc in the search box next to the Start button in Windows® and then press the Enter key.
- Import the certificate (see the Windows Help).
- Open the certificate by double-clicking it.
- Click the Details tab.
- Scroll down the Details list until you find the Thumbprint field.
- Click on the Thumbprint field and copy the Thumbprint value to the clipboard. The value is padded with spaces. You need to remove these spaces.
For more information about using Windows Certificate Manager, see the Windows Help.
- Paste the Thumbprint value into the PublisherThumbprint attribute in the AVEVA Insight Publisher file. The file has the name aahCloudConfigurator.exe.config. By default, the file is stored at the following location:
C:\Program Files\AVEVA\InsightPublisher\x64\aahCloudConfigurator.exe.config
The path will differ from the default if you have installed AVEVA Insight Publisher in a different folder.
Example:
The example below shows the Publisher Thumbprint attribute populated:

If you do not want to use a certificate, set the Publisher Thumbprint attribute to blank (see below):

Further Information