Exporting Historical Data to AVEVA Insight
You can export historic data for Geo SCADA Expert points and accumulators to the historians in various AVEVA applications, including AVEVA Historian (formerly Wonderware Historian) and AVEVA Insight (formerly Wonderware Online). Historic data is only exported for points and accumulators for which an AVEVA Historic Data Export item is specified in Export section of the configuration Form. Data that is subsequently stored in the historian will be exported to the historian in the specified AVEVA application. For more information about both of these requirements, see Define the Historic Export Details in the Geo SCADA Expert Guide to Core Point Configuration. Additionally, the AVEVA Historic Data Export driver has to be enabled and set up in Geo SCADA Expert (see Introduction to the AVEVA Historic Data Export Driver and see Configure an AVEVA Historic Data Export Item).
This section describes the procedure that you need to follow to connect Geo SCADA Expert to AVEVA Insight and to export historical data to that application.
To export historic data to AVEVA Insight, follow this procedure:
- Install AVEVA Insight Publisher on the Geo SCADA Expert server(s) from which historic data is to be exported to AVEVA Insight.
- Set the Historian field on the AVEVA Historic Data Export item to AVEVA Insight (Wonderware Online). For more information, see Specify the Direct Connection Properties.
- Before you can connect Geo SCADA Expert to AVEVA Insight, you will need to generate a connection token (see Generate a Connection Token with AVEVA Insight Publisher). The connection token will enable you to help secure the communications between the two applications. If your Geo SCADA Expert system has a Hot-Standby configuration, you need to install a security certificate before you generate the connection token. This is so that the token can be shared by more than one computer (see Use a Certificate for an AVEVA Insight Connection Token).NOTICE
Inability to export historic data
Do not use the 'Share' option offered by AVEVA Insight Publisher. This option is not currently supported by Geo SCADA Expert. Instead, you have to install a security certificate to enable a connection token to be shared by more than one computer in a Main-Standby server configuration.Failure to follow these instructions can result in the inability to export historic data to AVEVA Insight. - When you have generated the connection token (and installed the certificate, if necessary), use the Set Token pick action to enter the token into Geo SCADA Expert (see Set Token). For more information about using pick actions, see Object Menu in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.