Specify the Background Color used in Lists

This section applies to Lists other than Alarms Lists on ViewX clients.

Use the List Colors section on the Lists tab of the Options window to specify the colors used in the background of Lists, except the Alarms List:


To change the Background color:

  1. Click on the Background color.
    A pop-up color window is displayed.
  2. Either:
    • Select a color from the palette.

      Or:

    1. Select the ... option.
      The Color window is displayed.
    2. Use the Color window to define a color (see Using the Color Window).
    3. Select OK to close the Color window.

Example:

A ViewX client with this List Colors configuration:

Will result in a display like this:


If you select the Ignore Object Color check box:

The background colors specified for the objects are ignored and overridden by the selected color: