Errors When Create Devices Last Ran
Associated with: Sparkplug™ Edge Nodes
The Errors When Create Devices Last Ran status attribute is only displayed if the Create Devices from Device Birth Messages pick action has ever been executed on the selected Sparkplug Edge Node.
This status attribute indicates whether Geo SCADA Expert detected any issues when the Create Devices from Device Birth Messages pick action was last executed on the selected Sparkplug Edge Node.
A value of 0 (zero) indicates that the Device creation process that was last triggered by the Create Devices from Device Birth Messages pick action completed successfully.
If a value other than 0 is displayed, check the time and date that has been reported by the Device Configuration Error Alarm status attribute, and then look at the entries in the Alarms List and Events List from that time onwards to ascertain the issues that occurred. The entries will be assigned the Sparkplug Object Creation Error category (see Alarm and Event Categories that are Specific to the Sparkplug™ Driver).