Last Import Time

Associated with: Sparkplug™ Property Translation Tables

You create the content for the Property Translation Table outside of Geo SCADA Expert and then import the file into the database using the Import Property Translation Table pick action. This status attribute indicates when the Import Property Translation Table pick action was last used to successfully import a file into the selected Property Translation Table.

The status attribute displays one of these values:

If the last attempt to import a Property Translation Table into this database item did not succeed, look at the Events List to ascertain the issue(s) that occurred. The entries will be assigned the Sparkplug Object Creation Error category (see Alarm and Event Categories that are Specific to the Sparkplug™ Driver).

It is also possible for a file to be successfully imported, but contain errors. This can happen if the file contains valid information, but some of its entries are not applicable to a Sparkplug Property Translation Table (see Create the Content for a Property Translation Table). These errors are logged in the Events List for the Property Translation Table database item into which the file is imported.