Create Points from Birth Metrics

Associated with: Sparkplug™ Edge Nodes and Sparkplug™ Device items

Security permission required to access this pick action: Configure

NOTICE

unexpected impact on system performance

Use the Create Points from Birth Metrics pick action with care. Do not use the pick action to create points automatically on a Sparkplug Edge Node or Sparkplug Device that handles a large number of metrics. System operation could be adversely affected while automatic point creation is in progress for a Sparkplug Edge Node or Sparkplug Device with a birth certificate that contains thousands of metrics.
Failure to follow these instruction can impact adversely on system performance.

Use this pick action to create the relevant suite of Sparkplug Points in the database and automatically associate those points with the selected Sparkplug Edge Node or Sparkplug Device.

The Create Points from Birth Metrics pick action is only available on a Sparkplug Edge Node or Sparkplug Device item once Geo SCADA Expert has been in communication with the broker and has received the Sparkplug birth certificate for that Sparkplug Edge Node or Sparkplug Device. This status is indicated by each item's Birth Certificate status attribute.

You can optionally use the pick action in conjunction with a Property Translation Table. You use the table to specify which configuration properties Geo SCADA Expert is to set on the points when it creates them as a result of the Create Points from Birth Metrics pick action being executed. If you intend using a Property Translation Table, you have to create the content for that table outside of Geo SCADA Expert, then import it into the database and associate it with the relevant Sparkplug Edge Node or Sparkplug Device. You have to do this before using the Create Points from Birth Metrics pick action. For more information, see Create the Content for a Property Translation Table, and see Use a Property Translation Table to Configure Automatically Created Points.

You select the Create Points from Birth Metrics pick action to trigger Geo SCADA Expert to create a Sparkplug Point of the appropriate type for each suitable metric that is included in the cached version of that Edge Node or Device's birth certificate. The birth certificate includes information about the metrics (tags, or items of data) that exist in the Edge Node or Device. You then perform the same action on other Sparkplug Edge Nodes and Sparkplug Devices in your database as required.

We strongly recommend that you carefully check the suite of newly created points to confirm that they are of the correct point type and do map to the relevant metrics as intended. Also adjust the configuration of any newly created points that are to be output points (Geo SCADA Expert creates all of the points as input points).

If you used the Create Points from Birth Metrics pick action in conjunction with a Property Translation Table, check that the automatically set properties on the newly created points are configured as expected.

Edit the configuration of the newly created points as required. A message area at the bottom of each point's configuration Form will display messages relating to any invalid, incomplete, or conflicting configuration that requires addressing. For more information, see Mandatory Configuration and Invalid Configuration Messages in the Geo SCADA Expert Guide to Core Configuration, and see the point configuration topics in this driver guide.

If using this pick action with the Automation Interface, you need to specify the method name CreatePoints.

Further Information

Operational Limitations in the Sparkplug Driver.

To determine whether issues are detected when running the pick action, see: