Introduction to the Mitsubishi Driver
This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:
- Install and run the driver
- Ensure that the driver is licensed
- Configure the required database items and settings on the driver
- Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.
Intended Audience
This guide is primarily intended for engineers who are responsible for configuring Mitsubishi items and features in the Geo SCADA Expert database.
The guide also contains information of use to maintenance engineers.
The Mitsubishi Driver provides extra functionality to allow a Geo SCADA Expert system to be populated with data from, and control points on, Mitsubishi Slaves or Mitsubishi PLCs. The driver allows Geo SCADA Expert to communicate with:
- Mitsubishi Slaves
- The MELSEC A range of MitsubishiTM PLCs
(using Transmission Control Protocol Format 1) - Third-party PLCs that communicate using the Mitsubishi MELSEC A protocol.
Document Scope
This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s Mitsubishi driver (see Configuring Mitsubishi Devices in Geo SCADA Expert and see Mitsubishi Data Address Ranges).
It also explains the driver-specific status attributes. These attributes may be useful to system administrators and engineers when investigating unexpected system behavior (relating to the driver) (see Mitsubishi Specific Status Display Attributes).
This guide contains technical information that is intended for users that are sufficiently familiar with Geo SCADA Expert configuration and operation. Before reading this driver guide, ensure that you are familiar with:
- Geo SCADA Expert configuration practices, procedures, and the configuration of properties that are common to many database items. For more information, see the Geo SCADA Expert Guide to Core Configuration, and the Geo SCADA Expert Guide to Core Point Configuration.
- Driver structure, components, and configuration properties, pick actions, and status attributes that are common to many drivers. For more information, see the Geo SCADA Expert Guide to Drivers.
- Simple driver composition, configuration order, and configuration properties and logging options that are common to many simple drivers. For more information, see the Geo SCADA Expert Guide to Simple Drivers.
The Mitsubishi driver enables Geo SCADA Expert to communicate with slave devices and PLCs using the Mitsubishi MELSEC A protocol.
For information on how to configure Geo SCADA Expert to act as a Mitsubishi MELSEC A PLC and report any data changes back to its Master, see the Geo SCADA Expert Guide to the Mitsubishi Slave Driver.
There are no driver-specific pick actions for items on the Mitsubishi driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).
Geo SCADA Expert communicates with Mitsubishi PLCs using Transmission Control Protocol Format 1(see The Transmission Control Protocol Supported by Geo SCADA Expert).
For PLC information not covered by this guide, see the Mitsubishi documentation supplied with Mitsubishi PLCs.
For information on configuring Geo SCADA Expert so that it can communicate as a Mitsubishi Slave, see the Geo SCADA Expert Guide to the Mitsubishi Slave Driver.
Policy of Continuous Development
To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).