Configure an OPC UA Server

For every OPC UA server with which you want Geo SCADA Expert to communicate using the OPC UA protocol, you need to create and configure an OPC UA Server item in the database.

You use the fields on the OPC UA Server Form to configure the properties of the database item. The Form has several tabs, some of which contain properties that are common to many database items, and others that contain properties that are specific to OPC UA Servers.

The topics in this section document the properties that are on the Server tab.

Use the Server tab to:

The properties on the remaining tabs are common to many database items. For information about those tabs, see Tabs that are Common to Many Configuration Forms.