Introduction to the OPC UA Driver

This driver is supported by Geo SCADA Expert 2021 onwards. To use this driver, your Geo SCADA Expert servers and clients have to be running that version of Geo SCADA Expert software or later. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).

This driver is an advanced driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is intended for use by engineers who are responsible for the configuration of OPC UA specific items and features in Geo SCADA Expert. It can also be used by system administrators when investigating unexpected behavior relating to the OPC UA driver and operators who access the configured items.

Document Scope

The OPC UA driver is an OPC UA client. OPC UA is a platform-independent standard defined by the OPC Foundation, which enables interoperability between automation/control applications, field systems/devices, and business/office applications in the process control industry. Geo SCADA Expert supports a subset of the functionality defined by the OPC UA version 1.04 standard, to enable transfer of data between the Geo SCADA Expert server and third-party OPC UA compatible servers.

The OPC UA driver is used to read and write to data on other servers, including Geo SCADA Expert or third-party servers, using the OPC UA protocol. The driver supports the security that might be required to access particular items in an OPC UA server.

This guide explains how to configure OPC UA specific features and items within the Geo SCADA Expert database (see Configure OPC UA Items in Geo SCADA Expert).

It also explains driver-specific aspects that are of interest to system administrators and engineers when investigating unexpected system behavior relating to the OPC UA driver (see Status Attributes that are Specific to the OPC UA Driver, and see Driver Logging Options that are Specific to the OPC UA Driver).

There are driver-specific pick actions for items on the OPC UA driver (Using OPC UA Specific Actions). In addition, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).

Geo SCADA Expert includes several OPC drivers. For information on which driver is appropriate for your system requirements, see Which Driver?

Policy of Continuous Development

To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).

Further Information

OPC Foundation Standards: see www.opcfoundation.org