SMS Pager Service Alarm
Associated with: SMS Pager Services
The SMS Pager Service Alarm status attribute indicates the status of the SMS Service.
In normal conditions, Geo SCADA Expert will detect that the SMS Service is working correctly and has no alarms. In this situation, the SMS Pager Service Alarm status shows Enabled Inactive. If Geo SCADA Expert detects a problem with the channel, such as a failure or disconnection, the SMS Pager Service Alarm status will change to indicate that an alarm is raised.
Possible states: Displays one of the Standard Alarm States.
Further Information
For an example that demonstrates this status attribute, see Checking the Fail Count for Incoming SMS Commands.