Introduction to the SNMP Driver

This driver is a stand-alone driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported systems or devices. To interact successfully with such systems or devices, you need to:

Intended Audience

This guide is intended for use by all levels of user:

Document Scope

The SNMP documentation explains how to configure SNMP-specific features and items within the Geo SCADA Expert database (see Configuring SNMP Items in Geo SCADA Expert). It also explains how to:

There are driver-specific features that may be of interest to system administrators and engineers when investigating unexpected system behavior (relating to the SNMP driver). The driver-specific features include:

and driver-specific features that are of interest to operators using the system (see Using SNMP Specific Actions).

Operators can filter Alarm and Event Lists to display only those entries that are associated with SNMP Configuration Errors (see SNMP Specific Alarm and Event Categories).

The Simple Network Management Protocol (SNMP) is the standard network operations and maintenance protocol. The SNMP protocol can be used to remotely monitor and manage networked devices over a Local Area Network (LAN) or Wide Area Network (WAN). The protocol can run on top of other protocols, other than TCP/IP.

The syntax used for SNMP is Abstract Syntax Notation 1 (ASN.1). The syntax is used, for example, to define the type of data that is being retrieved using the SNMP protocol. The protocol works by using software ‘agents’ that are embedded into the networked devices in order to monitor various aspects of network status, such as events, network traffic, or device status. The SNMP driver acts as an SNMP Manager to retrieve such data from the SNMP agents, or control the data values. Geo SCADA Expert’s SNMP driver supports SNMP version 1, 2 and 3.

Using Geo SCADA Expert’s SNMP driver, you can retrieve current point data (by specifying a Poll action), or alarms and significant events (by specifying a Trap action—see Understanding TRAPS and INFORM Requests). You can also specify whether users can set data values at the SNMP agents.

For a list of data types supported by Geo SCADA Expert, see ASN Data Type.

Policy of Continuous Development

To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).