Original WebX Status Information
Geo SCADA Expert 2025 will be the last version of the product to support and include the deprecated Original WebX client. For web client support, please use Virtual ViewX clients instead of Original WebX clients.
The Server Status Tool provides status information that is organized into groups of categories, each of which contains sub-categories. The WebX group provides status information about any Original WebX clients that are connected to the server and the cookies, links and threads that they use.
The WebX group contains the following sub-categories:
- Clients (WebX)—provides status information about each Original WebX client that is connected to the server.
- Cookies—provides status information about each Original WebX cookie that is currently in use.
- Links (WebX)—provides status information for the connections between the server and any Original WebX clients.
- Threads—provides status information about the threads that are used to service the Original WebX links (links between the server and the Original WebX clients).
Further Information
Original WebX: see WebX Client.
Is WebX activity causing a high load on the server? see Original WebX Client Activity.