Introduction to the Sparkplug Publisher Driver
This driver is supported by Geo SCADA Expert 2025 onwards. To use this driver, your Geo SCADA Expert servers and clients have to be running that version of Geo SCADA Expert software or later. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).
This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:
- Install and run both the extension driver and its 'parent' driver (and, if applicable, its 'grandparent' driver)
- Ensure that the extension driver and its 'parent' driver (and, if applicable, its 'grandparent' driver) are licensed
(some extension drivers are licensed separately to their 'parent' driver) - Configure the required database items and settings on the 'parent 'driver (and, if applicable, the 'grandparent' driver)
- Configure the required database items and settings on this extension driver.
- Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.
Intended Audience
This guide is primarily intended for engineers who are responsible for configuring Sparkplug Publisher driver items and features in the Geo SCADA Expert database.
The guide also contains information for operators and maintenance engineers.
Document Scope
This guide explains the configuration, features and database items that are specific to the Sparkplug Publisher driver in Geo SCADA Expert. The driver provides Geo SCADA Expert with the ability to communicate with MQTT brokers in order to publish data to Sparkplug Host Applications.
This guide contains technical information that is intended for users that are sufficiently familiar with Geo SCADA Expert configuration and operation. Before reading this driver guide, ensure that you are familiar with:
- Geo SCADA Expert configuration practices, procedures, and the configuration of properties that are common to many database items. For more information, see the Geo SCADA Expert Guide to Core Configuration, and the Geo SCADA Expert Guide to Core Point Configuration.
- Driver structure, components, and configuration properties, pick actions, and status attributes that are common to many drivers. For more information, see the Geo SCADA Expert Guide to Drivers.
- The database items and configuration that are specific to this extension driver's 'parent' driver, along with any pick actions, status attributes, and logging options that are specific to that 'parent' driver. (Unless stated otherwise, this extension driver supports the features and options that are supported by its 'parent' driver, in addition to the features and options that are described in this extension driver guide.)
Some sections of this guide are intended for operator-level users. These sections are intended for users that are familiar with the navigational and operational aspects of Geo SCADA Expert. Before reading the operational sections in this guide, ensure that you are familiar with:
- The Geo SCADA Expert user interfaces (ViewX and Virtual ViewX), the various types of display, their navigation and operation. For more information, see the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
POTENTIAL SECURITY BREACH
The Sparkplug Publisher driver is an MQTT extension driver. It provides Geo SCADA Expert with the ability to communicate with Sparkplug compliant MQTT brokers in order to publish data to Sparkplug Host Applications. For such communications, Geo SCADA Expert needs to run both the MQTT driver and the Sparkplug Publisher extension driver (see Confirm that the Sparkplug Publisher Server Component is Installed).
Use this Geo SCADA Expert Guide to the Sparkplug Publisher Driver alongside the Geo SCADA Expert Guide to the MQTT Driver. As much of the information in the latter guide is assumed knowledge, we recommend that you read the Geo SCADA Expert Guide to the MQTT Driver before reading this driver guide.
Policy of Continuous Development
To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).