Virtual ViewX Server Setup Wizard

You use the Virtual UI Server setup wizard to install a Virtual ViewX server.

The Welcome page is the first page of the installation wizard. It provides you with information about the version of Virtual ViewX that you are about to install.

Virtual ViewX is supported by Geo SCADA Expert 2019 onwards. We strongly recommend that you install the Virtual ViewX server on a different machine to the Geo SCADA Expert server. This is to avoid potential performance issues due to the number of resources that each application uses.

If you do install Geo SCADA Expert and Virtual ViewX on the same machine, both applications must have the same version and build number. This is because the applications share some resources.

Unless specified otherwise, this topic summarizes the content of the Virtual UI Server window when the application is installed on a server operating system. The properties and pages differ slightly when the application is installed on a desktop operating system (see Servers and Desktop Computers, and see 64-Bit).

  1. On the Virtual ViewX Setup Wizard page select Next, the installation process begins.

  2. To install the Virtual ViewX server, you need to review the license agreement and agree to the terms stated.

  3. Please read the End-User License Agreement and select the I acknowledge the terms in the License Agreement option.

    If you do not agree to the stated terms, select I do not acknowledge the terms in the License Agreement. You will be unable to install the Virtual ViewX Server features and the installation process will end.

  4. Select Next to proceed to the Custom Setup page.

  5. Use the drop-down button on the branch or individual component to include or exclude a component (or entire collection of components). Choose from the following options:

    • Will be installed on local hard drive—The selected component will be installed. If the component has sub-components, only those that are also selected will be installed.
    • Entire feature will be installed on local hard drive—The selected component and all of its sub-components will be installed.
    • Entire feature will be unavailable—The component will not be installed.

    With the runtime components that are not installed by default, if you intend to install any such components, you must purchase a license for them to be operational. Please contact your Schneider Electric sales representative for more information.

    Only install the Sentinel System Driver component if you are using a USB dongle to license the Virtual ViewX Server.

    Only install the SAP Crystal Reports component if you want the users of Virtual ViewX clients to be able to view and download generated Crystal reports.

  6. Select Next to proceed to the Configure the Website page.

    The Configure the Website page is only displayed on new Virtual ViewX installations on a server operating system. On upgrades and on a desktop operating system, you are taken directly to the Ready to Install page from the license agreement page.

    The Configure the Website page prompts you to configure the SSL settings for the Virtual ViewX website.

     

    SSL Port

    Enter the port number that you want to associate with the HTTPS service hosting the Virtual ViewX application. You can enter any port number apart from HTTPS port numbers that are already in use on the Virtual ViewX server machine (for example, web applications, including the Geo SCADA Expert server will often use HTTPS port 443). The default port number is 453.

    SSL Certificate

    Use the SSL Certificate field to specify the publicly signed or self-signed certificate for the SSL port connections. If available, the combo box will offer any public certificates that are installed, or previously generated self-signed keys that exist (for example, from a previous installation of Virtual ViewX, or IIS-hosted WebX). (You will not be offered any Original WebX certificates.) If none of these exist, the installation process will create a new self-signed certificate using the machine name.

    We recommend that you obtain a public certificate from a certificate authority (CA).

    Alternatively, you can either:

    • Obtain a public signed certificate from a zero cost provider.
    • Create a self-signed certificate.

    For more information, see the Geo SCADA Expert Knowledge Base.

    Use the 'Manage Computer Certificates' app in the Control Panel to install the certificate, then use IIS Manager's 'Bindings' configuration to configure IIS to use that certificate.

    For information about using HSTS, see Virtual ViewX Security.

    If you want to install a Certificate later you need to use the IIS Manager. Refer to your System Administrator for more information about adding Certificates and using IIS Manager.

    Allow Unencrypted Connections

    When you allow unencrypted connections, clients can connect over an HTTP connection instead of an HTTPS connection.

    Clear this check box (the recommended option) if the Virtual ViewX server is not to allow interactions with any client connections that are not encrypted.

    While we do not recommend it, select this check box if the Virtual ViewX server is to allow interactions with unencrypted client connections.

    HTTP Port

    This field is disabled, by default and is populated with the port number that is associated with the HTTP service that is hosting the Virtual ViewX application. This port number is different from the port numbers that are already in use on the Virtual ViewX server machine (for example, web applications, including the Geo SCADA Expert server will often use HTTP port 80).

    If you initially configure, but later decide to disable, the HTTP port, you should edit the web configuration file to specify that cookies should only be transmitted over a secure channel (see Make Cookies Secure).

  7. Select Next to proceed to the Configure the Server page.

    The Configure the Server page is only displayed on new Virtual ViewX installations on a server operating system. On upgrades and on a desktop operating system, you are taken directly to the Ready to Install page from the license agreement page.

    The Configure the Server page allows you to change the default website:

    Disable "Default Website"?

    Select the check box to disable the default website installed with IIS to free port 80 for Geo SCADA Expert.

    Clear the check box if you require the default website installed with IIS to appear.

  8. Select 'Install' to proceed to the Ready to Install page.

  9. When you have reviewed the settings shown on the Ready to Install page, select the Install button to start the installation process.

  10. When the installation is complete, the Finish page is displayed.

  11. Select Finish to complete the installation procedure.

Having installed the Virtual ViewX server, you will need to License your Virtual ViewX Installation. You will also need to Configure a Virtual ViewX Server Connection to the Geo SCADA Expert Server.

NOTICE

INABILITY TO RUN Virtual ViewX

Do not delete, or change the password of, the VVXLocalUser that is created automatically in Windows when Virtual ViewX is installed on the Virtual ViewX server. This user account is required to run the ViewX processes on that server machine. For more information, see User Accounts Created Automatically on the Virtual ViewX Server Machine.
Failure to follow these instructions can result in inoperable equipment.