Display Default View

This option is only available if:

  • You are accessing the Object menu for a Group, Group Instance, or Group Template.
  • That Group, Group Instance, or Group Template is configured to have a Default View (see Defining a Default View).

Select the Display Default View option to display the ‘file object’ (such as a Mimic or Trend) that is configured as the Group, Group Instance, or Group Template’s Default View.

Use the Default View to ascertain further information about the items within the Group and/or access alarm response actions and controls.

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.

Also see Display Help View, and see Display Alarm View.