Integration with SmartConnector - Planning

The goal of this integration is two different architectures with PME system and SmartConnector.

Architecture 1: SmartConnector (EWS server) exports the historical and alarm data to PME system (EWS client).

Architecture 2: SmartConnector (EWS client) imports the historical and alarm data from PME system (EWS server).

This integration planning section includes the following topics:

NOTE: The deployment of this integration requires application engineering expertise in installing and configuring SmartConnector and PME.