Manual Data Editor

TIP: You can open Manual Data Editor in Management Console from the Tools > System > Manual Data Editor link.

Use Manual Data Editor to edit logged measurement data or to manually enter measurement data into the PME database. With this tool, you can adjust incorrect data, outliers, roll overs, jitter, and other unexpected or unwanted data records. You can fill data gaps or enter manually collected data, such as clipboard readings from mechanical meters. The Manual Data Editor also has the ability to create new, custom measurements in PME.

NOTE: Manual Data Editor can only be used to edit trend data logs. It cannot be used to edit waveform logs or event logs.

notice

LOSS of data

Back up the database before making manual database edits.

Failure to follow these instructions can result in permanent loss of data.

 

For information on how to use the Manual Data Editor , see:

For reference information see: