Changing a report subscription

Change report subscriptions to update the subscription properties such as subscription name, output format, delivery mode, or subscription schedule.

To change a report subscription:

  1. In Reports, open the Report Library and select Manage Subscriptions from the Options menu at the top of the Library. This opens Manage Subscriptions.
  2. In Manage Subscriptions, find the subscription you want to change. All existing subscriptions are displayed in the subscriptions table.
  3. To view the options for the subscription, click Edit Subscription to open the Modify Subscription dialog.
  4. In Modify Subscription, change the options in the dialog and click Save to update the subscription.
  5. Click Close.

Related topics:

Reports:

Subscriptions:

Other

For information on how to use Reports, see Reports.