Add tags and devices to your system

On the Profile Editor > Define Device Type Tags tab, follow these general steps to add tags and devices to your system:

  1. Manage the units and unit conversions that you will use (such as amperes into milliamperes), see Add or Edit a Base Engineering Unit or Conversion.
  2. Add and edit custom tags, see Setting up custom tags.
  3. Add or edit device types, see Managing device types.
  4. Establish device type categories and subcategories, used in reporting, see Printing the .CSV file.
  5. Edit tag addresses, see “About tags”.