After migrating the software
Perform the following procedures after you migrate the PME software.
Activate software licenses
notice
LOSS of communication
| ● | Activate product and component licenses prior to the expiry of the trial license. |
| ● | Activate sufficient licenses for the servers and devices in your system. |
| ● | Export the existing hierarchy template out of Power Monitoring Expert before importing a new template. The new template can overwrite the existing template, which can permanently remove all information contained in the original. |
| ● | Backup or archive any SQL Server database data before adjusting any database memory options. |
| ● | Only personnel with advanced knowledge of SQL Server databases should make database parameter changes. |
Failure to follow these instructions can result in loss of data.
After you are satisfied with the new system, return your old licenses and then activate the licenses on the new PME system.
NOTE: After you return the licenses, the old system is no longer functional.
For information on how to activate licenses, see Licensing configuration. For general information on licensing, see Licensing.
(Recommended) Restart the system
Restart (reboot) your system.
Verify correct database behavior
Verify that the system can access the databases by checking configuration settings and historical data logs. Confirm that the amount of historical data in the database is as expected. Use the database backups to restore any data that might have been deleted or lost, accidentally, during the migration.
notice
LOSS of data
| ● | Back up the database at regular intervals. |
| ● | Back up the database before upgrading or migrating the system. |
| ● | Back up the database before trimming it. |
| ● | Back up the database before making manual database edits. |
| ● | Verify correct database behavior after making database or system changes. |
Failure to follow these instructions can result in permanent loss of data.
Cybersecurity
Review the cybersecurity information. See Cybersecurity for details.
Windows Integrated Authentication for SQL Server
If you installed the new PME system with Windows Integrated Authentication, see Windows Integrated Authentication for SQL Server for post-install configuration steps.
Check services
Open the Windows Services dialog and ensure that all of the necessary
For more information the
(For Standalone architecture only) Review Windows Task Scheduler
The Windows Task Scheduler has preconfigured scheduled jobs for performing backups, maintenance, size notification, trims, and archiving (on the ION_Data database) on the PME databases. Review these schedules and make any modifications that you require.
For more information on Database Manager and Windows Task Scheduler, see Database Manager.
Check IIS
Ensure that Internet Information Services (IIS) is working by typing the URL http://localhost/ in the address field of your browser to display an IIS image. In some cases, security restrictions may block access to this web page.
Set up Web Clients
Set up Web Client access in your browser, by entering the fully qualified domain name of the server hosting PME, or its IP address, followed by the path name. The path name is configurable during the install of the software. The default path name is /Web. Example: https://ServerName/Web or https://10.152.35.18/Web. For more information on Web Clients, see Client types.