Configure UPS Performance

UPS Performance includes the UPS Auto Test Report and the UPS Battery Health Report.

warning

inaccurate data results

Do not incorrectly configure the software or the devices.
Do not base your maintenance or service actions solely on messages and information displayed by the software.
Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.
Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

 

Configure the UPS Auto Test Report

To configure the UPS Auto Test Report:

  1. Set up the UPS devices in PME.

    NOTE: See Supported measurements and devices for information on supported UPS devices for this report.

  2. Set up the UPS ION framework in the VIP. See Setting up the UPS Auto Test ION framework in the VIP for details.
  3. Define the UPS devices in the UPS Configuration Tool.
  4. Define a Group in the UPS Configuration Tool and add the UPS devices to the group.
  5. Generate the Vista diagrams with the UPS Configuration Tool and configure the diagrams. See Setting up the Vista Diagram for UPS Auto Test for details.
  6. Open the report template in the Reports Web Application, set the report input parameters, and generate the report.

For information on how to use the report, see UPS Auto Test Report.

Configure UPS Battery Health Report

To configure the UPS Battery Health Report:

  1. Set up the monitoring device that records the battery voltage. See Set up the UPS Battery Health monitoring device for information on how to configure the device. See Supported measurements and devices for details on which measurements are required
  2. Open the report template in the Reports Web Application, set the report input parameters, and generate the report.

For information on how to use the report, see UPS Battery Health Report.