Defining utilities

A utility represents the logical utility provider that feeds a load under normal operation. This logical utility has no functional purpose in the calculations for power redundancy. It is used to provide a more complete diagram representation for the generator system. A system may have one or two utilities represented in the diagram.

To define a utility:

  1. Click the utility element in the diagram. The Properties screen appears.

  2. Complete the details for the utility:
    1. Utility Name: Enter a name for the utility.
    2. Description: Enter a description for the utility. This field is optional.
  3. Click Done to save the utility.

Once the configuration of the generators, loads, and utilities are complete, click Apply to save, or click OK to save the configuration and exit the utility.

Related Topics: