Defining generators

A generator represents an actual generator device. A group contains at least one generator and can contain multiple generators. For some system types, each group must contain the same number of generators. See Generator Power configuration restrictions for more information.

To define a generator:

  1. Click on the generator object border. The selected generator will be highlighted in blue and the Properties screen appears.

  2. Complete the details for the generator:
    1. Generator Name: Enter the name for the generator.

      This name must be unique for each generator in the system.

    2. Description: Enter a description for the generator. This field is optional.
    3. Nameplate Rating (kVA): Enter the maximum output power (kVA) of the generator. This value must be greater than zero.
    4. Derated Nameplate Rating (kW): Enter the maximum power capacity (kW) that the generator is expected to support. This value must be equal or less than the nameplate rating value, and greater than zero.
  3. Click Done to save the generator.

Related Topics: