Deleting an Alarms view
Delete Alarms views that are no longer needed.
To delete an Alarms view:
- In the alarm viewer, open the view library and navigate to the view you want to delete.
- Right-click the view name or click Options
for this view, and select Delete - In Delete Content, click Yes, to delete the view from the view library.
NOTE: You cannot delete system views or the System Views folder.
Related topics:
- Adding a new Alarms view
- Copying an Alarms view
- Editing an Alarms view
- Sharing an Alarms view
- Moving an Alarms view
- Deleting an Alarms view
- Setting a default Alarms view
- Changing the alarm viewer settings
- Deactivating alarms
For reference information see:
For information on how to use Alarms, see Alarms.