Setting a default Alarms view
The default Alarms view is the view that opens when you first open the Alarms application. You can set a default for your own workspace or the entire system.
NOTE: Access to this application or function is controlled by user privileges.
To set a default Alarms view:
- In the alarm viewer, open the view library and navigate to the view you want to set as default.
- Right-click the view name or click Options
for this view and select Set as default. This opens the Configure Default Item dialog. - In Configure Default Item, enable Set as my default or Set as system default.
- Click OK to save the default settings.
Related topics:
- Adding a new Alarms view
- Copying an Alarms view
- Editing an Alarms view
- Sharing an Alarms view
- Moving an Alarms view
- Deleting an Alarms view
- Setting a default Alarms view
- Changing the alarm viewer settings
- Deactivating alarms
For reference information see:
For information on how to use Alarms, see Alarms.