Software Modules
Software modules combine different software features and capabilities to create a specific set of deliverables. Software modules are designed around a particular application. Examples of software modules include the Power Quality Performance Module, the Energy Analysis Reports Module, and the Breaker Performance Module.
This section provides information on how to use the Software Modules in Power Monitoring Expert.
Use the links in the following table to find the module you are looking for:
| Module | Application |
|---|---|
| Backup Power Module operation |
Generator and Uninterruptible Power Supply (UPS) performance monitoring and reporting, including battery health. |
| Breaker Performance Module operation |
Circuit breaker aging and breaker settings monitoring. |
| Capacity Management Module operation |
Generator and Uninterruptible Power Supply (UPS) capacity monitoring and reporting. Includes transformer and UPS loss monitoring. |
| Energy Analysis Dashboard Module operation |
Gadgets for identifying consumption patterns and anomalies and for comparing different consumers over time. |
| Energy Analysis Reports Module operation |
Reports for energy consumption monitoring and modeling, including energy usage by process area or by product output. |
| Energy Billing Module operation |
Energy-based billing and reporting, including consumption monitoring and reporting at the branch circuit level. |
| Event Notification Module operation |
Notifications of power system events via email, SMS, or SNMP. |
| Insulation Monitoring Module operation |
Monitoring for isolated power systems, such as the ones found in hospital operating rooms. |
| Power Quality Performance Module operation |
Analysis of power quality events and disturbances and their impact on the monitored system. |