Viewing historical (trend) data
- Click the meter icon to open its diagram, then click the link or tab that contains the button for the trending information you want to view.
-
Click the Data Log Viewer button
that corresponds to the data log you want to view.
The data log table displays today's data by default.
When the data log table opens, 30 rows of data are displayed initially. As you scroll or page down, 30 additional rows of data at a time are added to the table.
-
Click Change Date Range to change the timeframe for the data and select one of the available options for the data that you want to view. To specify a custom date range, select Between these dates then click the calendar icons
to set start and end dates.
The new date range is applied when you view the graph. Click Show Table to return to the data log table. (When you return to the data log table, your previous table header selections are cleared.)
If you select a custom date range, a maximum of 6000 rows of data are displayed initially. If the custom date range includes more than 6000 rows of data, you can display the additional records in increments of 30 rows at a time by scrolling down or pressing End.
- Select the check boxes for the items in the table header for the parameters that you want to graph.
- Click Show Graph.
- Manipulate and control the displayed graph by doing the following:
- To zoom in on the graph, left click and drag the mouse pointer around the portion you want to zoom in on.
- To restore the graph to its original display size, double-click anywhere in the graph.
- Click:
- Device Diagram to return to that page.
- Change Date Range to select a different date range for the data log table. The new date range is applied when you view the graph.
- Show Table to return to the data log table. (When you return to the data log table, your previous table header selections are cleared.)
RMS waveform plotting
The Diagrams application plots the calculated root mean square (RMS) values for waveforms.
Related topics:
- The Diagrams user interface
- User authentication
- Viewing historical (trend) data
- Viewing meter events
- Viewing user diagram of devices with security
- Performing manual control actions
- Stale data and error indicators
- Power Quality Performance diagrams
- Insulation Monitoring diagrams
- UPS Auto Test diagrams
- EPSS diagrams
- Breaker Aging diagrams
For information on how to configure Diagrams, see Diagrams and graphics configuration.