Power Quality Reports
NOTE: The Power Quality Analysis and Power Quality Impact reports are part of the Power Quality Performance Module. This module requires a separate license.
PME includes the following power quality report templates:
- EN50160:2000 Report
- EN50160:2000 Mains Signaling Report
- EN50160:2010 Report
- EN50160:2010 Mains Signaling Report
- Harmonic Compliance Report - Legacy
- Harmonic Compliance Report
- IEC61000-2-4 Report
- IEC61000-4-30 Report
- Power Quality Report
- SARFI Report
- Power Quality Analysis Report
- Power Quality Impact Report
CAUTION
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
Failure to follow these instructions can result in injury or equipment damage.