Integration with EcoStruxure Building Operation - Configuring
Configuring the PME/EBO Integration solution includes the following steps:
- Configuring server settings
- Configuring communications
- Configuring PME Web Applications
- Integrating PME Web applications in Building Operation
- Setting up Graphics in Building Operation
- Configuring Dashboards and Slideshows
NOTE: These steps are required for both solution architectures, unless specifically called out in the workflow steps.
See the following sections for details.