Dashboards configuration
Use the Dashboards application to view high level historical and real-time data, for example Key Performance Indicators (KPIs). The information in the Dashboards application is accessed through dashboards with gadgets. Dashboards are saved in the Dashboard Library. In addition to viewing individual dashboards, you can create slideshows to automatically display a sequence of dashboards.
warning
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
| ● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
Open the Dashboards application from the Dashboards link in the Web Applications banner.
For information on how to configure the Dashboards application, see:
Dashboards:
- Adding a new dashboard
- Editing a dashboard
- Sharing a dashboard
- Moving a dashboard
- Deleting a dashboard
- Set default options for a dashboard
- Configuring a slideshow
Gadgets:
For reference information see Dashboards user interface (UI).
For information on how to use Dashboards, see Dashboards.