Energy Analysis Dashboard Module design
The Energy Analysis Dashboard Module includes dashboard gadgets that help you break down consumption by load type, visualize consumption cost, and do an 80/20 analysis to identify the largest consumers. You can identify consumption patterns and anomalies and compare different consumers over time.
Components
The following gadgets are part of this module:
- Aggregated Consumption Ranking gadget
- Aggregated Pareto Chart gadget
- Consumption Ranking gadget
- Heat Map gadget
- Pareto Chart gadget
- Sankey gadget
Prerequisites
- The gadgets need consumption data, for example electrical consumption (kWh) or WAGES (water, air, gas, effluent, steam) consumption.
- The consumption measurement data for the gadgets must be available as historical data logs in the database.
- For the Sankey gadget you need to set up a hierarchy for the input measurements. See Hierarchy Manager for information on setting up a hierarchy.
Design Considerations
No special design considerations.
Related topics:
Energy Analysis Dashboard Module topics
- Energy Analysis Dashboard Module design
- Energy Analysis Dashboard Module configuration
- Energy Analysis Dashboard Module operation
Other software features
Other Software Modules