Capacity Management Module Design
The Capacity Management Module provides generator, Uninterruptible Power Supply (UPS), and general equipment monitoring and reporting. It also includes transformer and UPS loss monitoring and reporting. The losses are reported in terms of energy and cost.
Components
The following applications and features are part of this module:
Reports:
- Branch Circuit Power Report
- Equipment Capacity Report
- Generator Capacity Report
- Generator Power Report
- Power Losses Report
- UPS Power Report
Tools:
- Generator Performance Configuration Tool
- Generator Power Configuration Utility
- UPS Power Configuration Utility
- Power Losses Configuration Utility
Diagrams:
- Equipment Vista Diagrams
Prerequisites
- The measurement data for the reports must be available as historical data logs in the database before running the report.
- This module requires a separate license. See Licensing for more information.
Report | Needs |
---|---|
Branch Circuit Power Report |
(See Supported measurements and devices for more information.) |
Equipment Capacity Report Generator Capacity Report |
(See Supported Measurements and Devices for more information.) |
Generator Power Report |
(See Supported Measurements and Devices for more information.) |
Power Losses Report |
(See Supported Measurements and Devices for more information.) |
UPS Power Report |
(See Supported Measurements and Devices for more information.) |
Design Considerations
- Some of the reports only work with certain device types.
Related topics:
Capacity Management Module topics
- Capacity Management Module design
- Capacity Management Module configuration
- Capacity Management Module operation
Other software features
Other Software Modules