Other software licensing
PME can be used with a number of third party, add-on applications. These applications can be integrated with PME or can be used standalone. Check the licensing requirements of these applications before using them with PME.
Third party software licenses for add-on applications are not included in the PME license. Schneider Electric does not resell third party add-on licenses.
Examples of third-party add-on applications include:
- Microsoft Office
- Virtual Machine software
- Third party OPC server/client software
- Virus and malware detection and application control software
Related topics:
- Licensing overview
- Licensing process
- Licensing tools
- Important notes on licensing
- Operating System licensing
- SQL Server Licensing
- Other software licensing
- Licensing configuration
For reference information see: