SQL Server Licensing
PME is designed to operate with a Microsoft SQL Server database system. See Operating Environment for a list of supported Microsoft SQL Server versions and editions.
Microsoft SQL Server is available as a free, scaled down Express version, and as a licensed, full server version. You can use both versions with PME. For information on the limitations when using SQL Server Express, see SQL Server considerations.
A free version of SQL Server Express is included in the PME installation files and you have the option to install it during the installation of PME.
You can purchase licenses for a full server version from Microsoft or from 
Related topics:
- Licensing overview
- Licensing process
- Licensing tools
- Important notes on licensing
- Operating System licensing
- SQL Server licensing
- Other software licensing
- Licensing configuration
For reference information see: