Dashboards
warning
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
| ● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
TIP: You can open the Dashboards application from the Dashboards link in the Web Applications banner.
Time display
See Time Display in Web Applications for information on how time is displayed in a system where the monitoring devices, the PME/Web server, and the Web client (browser) are in different time zones.
For information on how use the Dashboards application, see:
For reference information see:
For information on how to configure Dashboards, see Dashboards configuration.