Backing up Power Monitoring Expert
This section provides information on backing up the following necessary Power Monitoring Expert components:
- Power Monitoring Expert databases
- Power Monitoring Expert config folder
- Power Monitoring Expert diagnostics
When backing up Power Monitoring Expert (PME), the following assumptions are made:
- The backup applies to a standalone server implementation.
- That the new PME server has the same name as the original.
- That the same version of PME and SQL Server are used on both the new and old servers.
- The backup does not include the following items, which can be configured again for a new instance:
- Dashboard Images
- Dashboards
- Data Center Edition Images
- Database archives
- EWS config
- Report Subscriptions
- SQL Script Files