Web Applications settings
TIP: You can open the Settings page from the SETTINGS link in the Web Applications banner.
Use the Settings page to access Web Applications settings and configuration tools.
NOTE: Access to this application or function is controlled by user privileges. See Managing user accounts, role names, and mapping for details.
TIP: Use Search, in the Settings Library, to find the settings and tools you are looking for based on keywords.
The Settings page consists of a Settings Library and a configuration area. The Settings Library provides access to the following settings and tools:
| Category | Settings/Tools |
|---|---|
| Alarms | Alarm Views
|
| Integrations | Authorized Hosts |
| Personalization | Personal Preferences
System localization System Theme |
| Security | Session timeout |
| Web Redundancy | Web redundancy |