Plant SCADA Migration Information

This section contains the required and optional steps to migrate from pre-7.x versions of Plant SCADA to Power Operation. For an overview, see Migrating from Plant SCADA (formerly Citect SCADA).

NOTE: It is possible to restore and run the Citect project and includes on Power Operation and modify them to fully convert them to Power Operation projects. However, we recommend using the following migration steps to take advantage of the built-in power management features of Power Operation.

The required migration steps are:

  1. Create a New Project
  2. Import Citect Customizations
  3. Create Device Type Tags and Devices
  4. Export Alarm History
  5. Enable Waveforms

The optional migrations steps are:

  1. Re-create One-line Animation
  2. Add Notifications
  3. Add Basic Reports and LiveView
  4. Set Up Two-Factor Authentication