OPC – UA

It is possible to use an OPC server (Data Access) in conjunction with EcoStruxure Machine Expert Twin. Select this option if that is the device being used.

As part of the basic psychics model example guide, we show how to use an OPC Server to test the model.

Properties

  • Identification
    • Name – Customiszable name
    • Id – Customizable id
  • Communication
    • Auto Connect
  • Host
    • Address – address of the device running the server
Previous Fetch and Write
Next Serial (RAW)