METHOD SetCommunicationState : ERROR
Starts, stops or resets a device
Use IDevice2.CheckSupportedCommunicationState and IDevice2.CheckCurrentSupportedCommunicationState to check which transitions are possible!
Scope
Name
Type
Comment
Return
SetCommunicationState
ERROR
Input
eRequestedState
DEVICE_TRANSITION_STATE
desired transition