FUNCTION_BLOCK ETrigTlTo EXTENDS ETrigTl IMPLEMENTS IETrigTlTo
Base implementation of a PLCopen Edge Triggered Behavior Model (see: IETrigTlTo)
For use, this block should be extended and the specific inputs and outputs must be supplemented. The output eErrorID of the application-specific enum type ERROR must be added.
InOut: |
|
Properties:
ActionController, inherited from TimingControlledBehaviourModelBase
ModelTimeLimit, inherited from ETrigTl
Methods:
AbortModel, inherited from TimingControlledBehaviourModelBase
CleanupAction, inherited from TimingControlledBehaviourModelBase
CyclicAction, inherited from TimingControlledBehaviourModelBase
ExitAction, inherited from TimingControlledBehaviourModelBase
GetConfiguration, inherited from TimingControlledBehaviourModelBase
GetConfiguration2, inherited from TimingControlledBehaviourModelBase
ResetAction, inherited from TimingControlledBehaviourModelBase
ResetModel, inherited from ETrigTl
SampleAction, inherited from EdgeTriggeredTimingControlledBehaviourModelBase
StartAction, inherited from TimingControlledBehaviourModelBase
StartModel, inherited from ETrigTl
Structure: