Data logging
The meter has a default, comprehensive data-logging configuration. Information regarding the default logging capacity and default logging configuration can be found in Default logging capacity.
To learn more about the Data Recorder modules in your meter, refer to the ION Reference.
Configuring data logging
Use Power Monitoring Expert or ION Setup to change your meter’s logging settings.
Using the front panel
You cannot configure logging using the front panel.
Using ION Setup
- Open the Setup Assistant for your meter. See the ION Setup Help for instructions.
- Select the Logging folder.
Use the Memory, Load Profile, and Event Log screens to configure your logging settings.
Memory screen
- Click Logging > Memory to re-allocate meter memory.
- Select the log you want to configure and click Edit. You can change both the Log Duration (days) and the Log Size (records). Changing these parameters affects the meter memory allocated to that log.
Load Profile screen
- Click Logging > Load Profile to configure the Revenue Log.
- Click the Channels tab to access the Revenue Log sources. Select a source.
- Click Unlink to unlink the parameter from the source.
- Click Edit to edit the parameter. The Parameter Selection dialog box displays the source register groupings. To view the individual registers, expand the node beside the register group . Select the register that you want to connect to the source, and then click OK.
Select the Show all available registers check box for a complete list of all possible registers.
- Click the Interval/Depth tab to edit the Revenue Log interval and duration and missing record handling.
Events screen
- Select the Event Log screen to configure what events are logged and the notification settings
- Click the Events tab, select a parameter and click Edit:
– Depth: This parameter sets the number of events the event log contains.
- Click the Notifications tab to configure the event log notification settings based on the number of unread entries. These settings allow you to define the designated reader and set a limit to the number of unread event log entries. Select a parameter and click Edit to change.
- Designated Reader: This parameter allows you to select a user to be the designated reader of the event log. An entry in the event log is designated unread until reviewed or backed up to external storage by the designated reader. This feature can assist in ensuring that event log entries are not overwritten before they can be reviewed.
- SMTP Server: This parameter displays the IP address of the SMTP Server. The value can only be displayed under this tab. Navigate to Communications > Advanced Ethernet > SMTP to change this setting. See Configuring Ethernet connections for information on configuring network settings.
- Depth: This parameter displays the number of events the event log can contain. The value can only be displayed under this tab. Navigate to Logging > Event Log > Events to change this setting.
- Unread Events: This parameter displays the number of event log entries that have not been reviewed or backed up to external storage by the designated reader. When the designated reader reviews the event log, this value returns to zero. If any user other than the designated reader reviews the event log, the unread events value does not change. This value is not configurable.
– Cutoff: This parameter determines the minimum priority level for events to be logged; events with a lower priority are not logged.
– EvPriority: This parameter sets the event priority of Sag/Swell events. See Configuring power quality event logging for more information.
– PhaseLossEnable: This parameter enables or disables phase loss event recording.
Changing waveform recording
The Waveform Recorder modules do not require changes to their default settings. If you want to change the format of the recorded waveforms, refer to the Waveform Recorder module description in the ION Reference.
NOTE: If you are generating COMTRADE waveform data records, the associated Waveform Recorder modules cannot be modified unless the COMTRADE module’s Module Enable register is set to DISABLED. If the Waveform Recorder modules are not configured identically (have the same setup register values) the COMTRADE module will not go online.
The default logging framework
The following sections outline the default logging capacity and configuration.
NOTE: The default logging configuration may be used by other components of your power monitoring system (for example, the reporting components of Power Monitoring Expert). Before you change the default configuration of any of the logs, ensure you understand the impact on the change on these components and the data they display.
Default logging capacity
The following table summarizes the default recording depths and recording intervals of the various Data recorders and Waveform recorders in the meter.
|
Log type |
ION8650A Default depth |
ION8650B Default depth |
ION8650C Default depth |
Interval |
|---|---|---|---|---|
| Energy logs | ||||
| Revenue log |
9120 |
6240 |
3360 |
900 seconds |
| Loss log |
9120 |
6240 |
N/A |
900 seconds |
| EgyDmd Log |
9120 |
6240 |
N/A |
900 seconds |
| Daily nominal log | ||||
|
DailyNom Log |
450 |
450 |
N/A |
Daily |
| Historic logs | ||||
| Hist Logs |
9120 |
6240 |
N/A |
900 seconds |
| Harmonic logs | ||||
| Harm Logs |
2280 |
1560 |
N/A |
3600 |
| Disturbance recorders | ||||
| Transient Log |
3000 |
N/A |
N/A |
Triggered on demand |
| Sag/Swell Log |
3000 |
3000 |
3000 |
Triggered on demand |
| SagSwellState Log |
3000 |
3000 |
N/A |
Triggered on demand |
| COMTRADE¹ |
1 |
N/A |
N/A |
Triggered by Waveform Recorder |
| EN50160 logs (ION8650A and ION8650B only) | ||||
|
14 Data Recorders |
Varies² |
Varies² |
N/A |
Daily, weekly, 10 minutes...² |
| 4-30 logs (ION8650A and ION8650B only | ||||
| 8 Data Recorders |
Varies³ |
Varies³ |
N/A |
3 second, 10 minute, 2 hour |
¹See the COMTRADE and ION Technology technical note for more details.
²See the Power Quality: ION Meters and EN50160 technical note for more details.
³See the IEC 61000-4-30 Compliance and ION meters technical note for more details.
Changing the log depths
Change the value in a Data Recorder module’s Depth setup register to increase the number of records stored in the recorder.
The RecordMode setup register controls how the Data Recorder overwrites old records; refer to the Data Recorder module description in the ION Reference before changing this setup register.
Logging frequency
The five Periodic Timer modules that control the frequency of different data recording are as follows:
- “Revenue Log Trg” controls the frequency of the logging of revenue values
- “Loss Log Trg” controls the frequency of Loss Compensation Data logging
- “EgyDmd Log Trg” controls the frequency of logging for the Energy and Demand Log (this log is used for generating reports using Web Reporter)
- “Hist Log Trg” controls the frequency of Historic Data logging
- “Harm Log Trg” controls the frequency of Harmonics logging
Programming your meter to write to any data recorder at continuous intervals lower than 60 seconds (heavy logging configuration) can cause loss of data in the event of a power failure.
notice
data Loss
Use an uninterruptible power supply (UPS) if you program your meter for heavy logging.
Failure to follow these instructions can result in data loss.
Change the value in the Period setup register to change the frequency of data logging (in seconds). Do not change the Sync Mode setup register.
Default logging configuration
The following sections describe each Data Recorder module and the parameters they log. Your meter may not have all the logs described and the settings may vary depending on the meter, its firmware and its template.
Revenue logging
The Revenue Log is configured for use with UTS MV-90 billing software. The default values logged by the Revenue Log are as follows:
|
Parameter |
Description |
|
kWh del int |
Interval kWh delivered |
|
kWh rec int |
Interval kWh received |
|
kVARh del int |
Interval kVARh delivered |
|
kVARh rec int |
Interval kVARh received |
Historic data logging
Three data recorders are used to record standard power system quantities, such as phase current, phase voltage and power factor. By default, they log the following output register values:
|
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Loss Log
One Loss Log recorder is configured to record loss values. By default, it logs the following parameters – note that the parameters differ depending on the meter template:
|
Template |
Loss Log parameter |
Description |
|
All |
MU Ia^2h int |
Phase A interval current squared hours |
|
All |
MU Ib^2h int |
Phase B interval current squared hours |
|
All |
MU Ic^2h int |
Phase C interval current squared hours |
|
35S only |
MU Vll ab^2h int |
Phase A interval voltage Line-to-Line squared hours |
|
35S only |
MU Vll bc^2h int |
Phase B interval voltage Line-to-Line squared hours |
|
35S only |
MU Vll ca^2h int |
Phase C interval voltage Line-to-Line squared hours |
|
9S/29S/36S only |
MU Vln a^2h int |
Phase A interval voltage Line-to-Neutral squared hours |
|
9S/29S/36S only |
MU Vln b^2h int |
Phase B interval voltage Line-to-Neutral squared hours |
|
9S/29S/36S only |
MU Vln c^2h int |
Phase C interval voltage Line-to-Neutral squared hours |
Harmonics logging
Two recorders provide various harmonics logs, including K-factor and Total Harmonics Distortion (THD). These recorders are labeled Harm Mean Log and Harm High Log. By default, they log the following values:
|
|
|||||||||||||||||||||||||
Energy Demand Log
One data recorder is configured to provide power system data for the Web Reporter component of Power Monitoring Expert.
|
EgyDmd Log |
|
|
kWh del |
kVAh del+rec |
|
kWh rec |
kW sd del-rec |
|
kWh del-rec |
kVAR sd del-rec |
|
kVARh del |
kVA sd del+rec |
|
kVARh rec |
PF lag mean |
|
kVARh del-rec |
PF lead mean |
Sag/Swell and Transient logging
Three data recorders provide details of these power quality events. The Sag/Swell and Transient data recorders, by default, log the following values:
|
Sag/Swell log (ION8650A and ION8650B) |
|||
|
DistDur |
DistV1Engy |
DistV2Engy |
DistV3Engy |
|
DistV1Min |
DistV2Min |
DistV3Min |
DistNominal |
|
DistV1Max |
DistV2Max |
DistV3Max |
SwellLim |
|
DistV1Avg |
DistV2Avg |
DistV3Avg |
SagLim |
|
Sag/Swell log (ION8650C) |
|
||
|
DistDur |
DistV2Max |
PT Prim |
|
|
DistV1Min |
DistV3Min |
PT Sec |
|
|
DistV1Max |
DistV3Max |
CT Prim |
|
|
DistV2Min |
DistNominal |
CT Sec |
|
|
Transient log |
|||
|
TranV1Dur |
TranV2Max |
TranNominal |
PT Sec |
|
TranV1Max |
TranV3Dur |
Threshold |
CT Prim |
|
TranV2Dur |
TranV3Max |
PT Prim |
CT Sec |
The SagSwellState data recorder provides additional information required by the Sag/ Swell and Transient logs.
See Configuring power quality event logging for enabling or disabling Sag/Swell and Transient events from being recorded in the Event Log.
NOTE: Modification of the Sag/Swell, Transient and SagSwellState logs is an advanced procedure that should only be performed by experienced users familiar with ION and the interaction of these data recorders.
See the COMTRADE and ION Technology technical note for information about COMTRADE records.
EN50160 compliance logging (ION8650A and ION8650B only)
By default, 14 Data Recorder modules are used for logging EN50160 compliance parameters.
|
|
The meter logs EN50160 counter data for present and previous observation periods as well as EN50160 events. Enable or disable EN50160 Parameter Logging via the default Power Quality diagram in the Vista component of Power Monitoring Expert.
For more information about EN50160 data logging, see the Power Quality: ION Meters and EN50160 technical note.
IEC 61000-4-30 logging (ION8650A and ION8650B only)
Eight data recorders are used to log parameters related to 4-30 compliance and to create reports.
| Data Recorder | 4-30 parameters logged |
|---|---|
|
4-30 3s THD Log 4-30 3s RMS Log 4-30 10mRMS Log 4-30 10mTHD Log 4-30 2hTHD Log 4-30 2hRMS Log 4-30 10s Freq 4-30 Intrp Log (disabled by default) |
– Voltage Disturbances – V1-RMS (Root-Mean-Square) – V2-RMS – V3-RMS – THD (Total Harmonic Distortion) – Vneg/Vpos – Vzero/Vpos – V-Overdeviation – V-Underdeviation – Frequency – Flicker (only available on A feature set) – Unbalance |
For more information on 4-30 compliance, see the IEC 61000-4-30 Compliance and ION meters technical note.
Viewing data log information
In ION Setup
- Select your meter.
- Select View > Data Screens > Data Recorders. The following logs are available for viewing, depending on your meter:
- Average Harmonics
- Energy & Demand
- Historic Average, Historic Highs, Historic Lows
- Maximum Harmonics
- Revenue Log
- Sags & Swells
- Transformer Losses
- Transients (ION8650A only)
See Reports for information on running basic reports in ION Setup.
In Power Monitoring Expert
You can view information from the data logs in the Vista, WebReach and Web Reporter components of Power Monitoring Expert. See Power Monitoring Expert help for more information.