Setting up Advanced security

Meter security has strong user login, user access management, and password complexity.

NOTE: We recommend that you use Advanced security mode.

For detailed information on the Advanced security mode capabilities, see Advanced security mode.

Prerequisites:

  • Meter connection using ION Setup.
  • Login credentials.
  • Security configuration access privileges.

To set up Advanced security:

  1. Open ION Setup > select the meter > Setup Assistant.
  2. Security > Security Mode > Edit. The Open Security Configuration file dialog box opens.
  3. Select the advanced.scf security configuration file.
  4. Click Open. If prompted, click Yes to use Advanced security.
  5. Next, either: