Configuring Daylight Saving Time advanced settings
Prerequisites:
To configure Daylight Saving Time (DST) advanced settings:
- Select > > .
- Select .
- (Optional) To manually set dates and times per year for DST, set Adjust for Daylight Saving time to Manual.
- Enter the Start Year and End Year; these years cannot exceed a 20 year range.
- If Adjust for Daylight Saving time is set to Manual, select a Start and End DST date and time for each year in the range.
- Select Apply.
- Select Save Working Copy.
- Synchronize changes.