Ethernet settings

Note: The available parameters and values may differ for your device.

Ethernet settings

Parameter Values Default Description
IPv4 Settings      
IP Address Contact your local network administrator for parameter values. 169.254.0.10 Specifies the TCP/IP Ethernet address.

Subnet Mask

Contact your local network administrator for parameter values. 255.255.0.0 The subnet mask address of your network.
Gateway Contact your local network administrator for parameter values. 0.0.0.0 The gateway IP address of your network.
SMTP Server Address Contact your local network administrator for parameter values. None The IP address of your SMTP server.
Ethernet      
Ethernet Device Name Contact your local network administrator for parameter values. <device type>-<last six digits of MAC address> The Ethernet Device Name is associated with your device when using DPWS. By default, it is the device type and the last six characters of the MAC Address.
Ethernet Receive Timeout Contact your local network administrator for parameter values. 3 Specifies the number of seconds the meter will wait for communication acknowledgments.
Modbus TCP Timeout Contact your local network administrator for parameter values. 0 Specifies the number of seconds the meter waits before disconnecting an idle Modbus TCP connection.
MAC Address Read-only Device dependent The device’s Media Access Control (MAC) address.
Protocols and ports      
DLMS Contact your local network administrator for parameter values.

4059

The assigned port for Device Language Message Specification (DLMS).
SSH/SFTP Contact your local network administrator for parameter values. 22 The assigned port for Secure Shell (SSH) and Secure File Transfer Protocol (SFTP) connections to the device.
DPWS Read-only 5357 The assigned port for Devices Profile for Web Services (DPWS).
WebServer (HTTP/HTTPS) Contact your local network administrator for parameter values. 80/443 The assigned ports for the device's web server.
Secure ION Contact your local network administrator for parameter values. 7443 The assigned port for Secure ION.
DNP Contact your local network administrator for parameter values. 20000 The assigned port for Distributed Network Protocol (DNP).
ION Contact your local network administrator for parameter values. 7700 The assigned port for ION.
Modbus RTU Contact your local network administrator for parameter values. 7701 The assigned port for Modbus RTU.
Modbus TCP Contact your local network administrator for parameter values. 502 The assigned port for Modbus TCP.
SNMP Contact your local network administrator for parameter values. 161 The assigned port for Simple Network Management Protocol (SNMP).