Digital alarm settings
Digital alarm settings
| Parameter | Values | Description |
|---|---|---|
| Label | Alphanumeric |
Sets the alarm label. |
| Alarm Active When | Input is ON, Input is OFF |
The digital input state that activates an alarm:
|
| Alarm Priority | None, Info Only, Low, Medium, High | Select the priority that you want to associate with the alarm. To stop an alarm from being displayed while keeping a record of the event, set the alarm priority to Info Only. |
| Custom | Enabled (1–255), Disabled |
Turn on Custom to define a specific alarm priority value. The available Custom priority value range depends on the Alarm Priority:
|