Alarms

An alarm is your device’s way of notifying you when it detects a condition. For example, an issue or an event that falls outside of typical operating conditions.

You can customize your device to generate and display high, medium, and low priority alarms. Your device also logs the alarm event information.

There are two configurable alarm types:

  1. Standard alarms
  2. Digital alarms